Keysight 89600 VSA .NET API
Equals Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > DisplayFontInfo Structure : Equals Method


Glossary Item Box

Determines whether the specified object is equal to the current DisplayFontInfo instance. (Overrides System.ValueType.Equals(System.Object).)

Overload List

OverloadDescription
Equals(Object)Determines whether the specified object is equal to the current DisplayFontInfo instance. (Overrides System.ValueType.Equals(System.Object).)  
Equals(DisplayFontInfo)Determines whether the specified object is equal to the current DisplayFontInfo instance.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also

Reference

DisplayFontInfo Structure
DisplayFontInfo Members
Base Implementation in Equals