Keysight 89600 VSA .NET API
Equality Operator
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > DisplayFontInfo Structure : Equality Operator


font1
The first instance of DisplayFontInfo to compare.
font2
The second instance of DisplayFontInfo to compare.

Glossary Item Box

Compares two DisplayFontInfo structures for equality.

Syntax

Visual Basic (Declaration) 
Public Operator =( _
   ByVal font1 As DisplayFontInfo, _
   ByVal font2 As DisplayFontInfo _
) As Boolean
C# 
public bool operator ==( 
   DisplayFontInfo font1,
   DisplayFontInfo font2
)
C++/CLI 
public:
bool operator ==( 
   DisplayFontInfo font1,
   DisplayFontInfo font2
)

Parameters

font1
The first instance of DisplayFontInfo to compare.
font2
The second instance of DisplayFontInfo to compare.

Return Value

true if the two instances contain the same information; otherwise, false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also