| Visual Basic (Declaration) | |
|---|---|
Public Operator <>( _ ByVal font1 As DisplayFontInfo, _ ByVal font2 As DisplayFontInfo _ ) As Boolean | |
| C# | |
|---|---|
public bool operator !=( DisplayFontInfo font1, DisplayFontInfo font2 ) | |
| C++/CLI | |
|---|---|
public: bool operator !=( DisplayFontInfo font1, DisplayFontInfo font2 ) | |
Parameters
- font1
- The first instance of DisplayFontInfo to compare.
- font2
- The second instance of DisplayFontInfo to compare.
Return Value
true if the two instances do not have the same information; otherwise, false.Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)