Keysight 89600 VSA .NET API
EnumUtilities Class Members
See Also  Methods 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : EnumUtilities Class

Glossary Item Box

The following tables list the members exposed by EnumUtilities.

Public Methods

 NameDescriptionMinimum SW Version
Public Methodstatic (Shared in Visual Basic)GetEnumAsInt32This method retrieves the value of the specified property as a 32-bit integer.  —
Public Methodstatic (Shared in Visual Basic)SetEnumFromInt32This method sets the value of the specified property from the supplied 32-bit integer.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also