Keysight 89600 VSA .NET API
Harmonic Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ExternalMixerSubband Class : Harmonic Property


Glossary Item Box

Gets or sets the harmonic to use for this band.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Harmonic As Integer
C# 
public abstract int Harmonic {get; set;}
C++/CLI 
public:
abstract property int Harmonic {
   int get();
   void set (    int value);
}

Remarks

Can only be set when the MixerType is set to Custom, otherwise an ArgumentInvalidException will be thrown.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also