Keysight 89600 VSA .NET API
LODoublerOn Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ExternalMixerSubband Class : LODoublerOn Property


Glossary Item Box

Gets or sets a value indicating whether the LO doubler is on for this sub band.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property LODoublerOn As Boolean
C# 
public abstract bool LODoublerOn {get; set;}
C++/CLI 
public:
abstract property bool LODoublerOn {
   bool get();
   void set (    bool value);
}

Remarks

Can only be set when the MixerType is set to Custom, otherwise an ArgumentInvalidException will be thrown.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also