Keysight 89600 VSA .NET API
FixedEqualizationValid Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FixedEqualizationValid Enumeration


Glossary Item Box

Is a data register valid for use in fixed equalization, or if not, why not.

Syntax

Visual Basic (Declaration) 
Public Enum FixedEqualizationValid 
   Inherits System.Enum
C# 
public enum FixedEqualizationValid : System.Enum 
C++/CLI 
public enum class FixedEqualizationValid : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EmptyNotValidRegister is empty—
InsufficientDataNotValidRegister has fewer than 5 points—
NotFreqDomainNotValidRegister does not contain frequency domain data—
NullNotValidRegister is null—
SegmentedDomainNotValidRegister has 2-D domain that is not Channel Domain; not usable for fixed equalization—
UninitializedNotValidRegister is uninitialized—
ValidRegister is valid for use in fixed equalization—
ZeroDeltaFreqNotValidRegister domain spacing is 0 Hz—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also