Keysight 89600 VSA .NET API
FrequencyMaskTriggerAmplitudeReference Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyMaskTriggerAmplitudeReference Enumeration


Glossary Item Box

Specifies whether mask amplitudes are absolute or relative.

Syntax

Visual Basic (Declaration) 
Public Enum FrequencyMaskTriggerAmplitudeReference 
   Inherits System.Enum
C# 
public enum FrequencyMaskTriggerAmplitudeReference : System.Enum 
C++/CLI 
public enum class FrequencyMaskTriggerAmplitudeReference : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AbsoluteThe mask amplitudes are absolute dBm value.—
RangeThe mask amplitudes are relative to the range of the trigger channel.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also