Keysight 89600 VSA .NET API
FrequencyMaskTriggerCriteria Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyMaskTriggerCriteria Enumeration


Glossary Item Box

Specifies the trigger criteria for the frequency mask trigger.

Syntax

Visual Basic (Declaration) 
Public Enum FrequencyMaskTriggerCriteria 
   Inherits System.Enum
C# 
public enum FrequencyMaskTriggerCriteria : System.Enum 
C++/CLI 
public enum class FrequencyMaskTriggerCriteria : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EnterTrigger occurs when the signal enters the region identified by FrequencyMaskTrigger.MaskToUse.—
EnterThenLeaveTrigger occurs when the signal enters and subsequently leaves the region identified by FrequencyMaskTrigger.MaskToUse.—
InsideTrigger occurs when the signal remains inside the region identified by FrequencyMaskTrigger.MaskToUse.—
LeaveTrigger occurs when the signal leaves the region identified by FrequencyMaskTrigger.MaskToUse.—
LeaveThenEnterTrigger occurs when the signal leaves and subsequently enters the region identified by FrequencyMaskTrigger.MaskToUse.—
OutsideTrigger occurs when the signal remains outside the region identified by FrequencyMaskTrigger.MaskToUse.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also