Keysight 89600 VSA .NET API
FrequencyMaskTriggerFrequencyReference Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyMaskTriggerFrequencyReference Enumeration


Glossary Item Box

Specifies whether mask frequencies are absolute or relative.

Syntax

Visual Basic (Declaration) 
Public Enum FrequencyMaskTriggerFrequencyReference 
   Inherits System.Enum
C# 
public enum FrequencyMaskTriggerFrequencyReference : System.Enum 
C++/CLI 
public enum class FrequencyMaskTriggerFrequencyReference : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AbsoluteThe mask frequencies are absolute.—
CenterThe mask frequencies are relative to the center frequency of the trigger channel.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also