Keysight 89600 VSA .NET API
FrequencyMaskTriggerMask Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : FrequencyMaskTriggerMask Enumeration


Glossary Item Box

Specifies which masks are used for the trigger.

Syntax

Visual Basic (Declaration) 
Public Enum FrequencyMaskTriggerMask 
   Inherits System.Enum
C# 
public enum FrequencyMaskTriggerMask : System.Enum 
C++/CLI 
public enum class FrequencyMaskTriggerMask : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BothSpecifies both upper and lower masks.—
LowerSpecifies the lower mask only.—
UpperSpecifies the upper mask only.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also