Keysight 89600 VSA .NET API
WindowAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > FrequencyVersusTime Class : WindowAuto Property


Glossary Item Box

Gets or sets a value indicating whether the window should be automatically determined based on the measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property WindowAuto As Boolean
C# 
public abstract bool WindowAuto {get; set;}
C++/CLI 
public:
abstract property bool WindowAuto {
   bool get();
   void set (    bool value);
}

Remarks

This setting is a boolean used to determine if the Window is automatically configured based on the measurement Window. If true, the TimeStep is automatically set to match the Window. If false, the TimeStep must be manually configured. The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also