Keysight 89600 VSA .NET API
DefaultSpan Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Frequency Class : DefaultSpan Method


Glossary Item Box

Sets the Span to its default value, which is the largest span supported by the current hardware.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub DefaultSpan() 
C# 
public abstract void DefaultSpan()
C++/CLI 
public:
abstract void DefaultSpan(); 

Remarks

When the current channel(s) can only be zoomed, then the span is changed to the largest supported value, but the center frequency is not changed. When the channel(s) can be baseband (IsZoom is false), then the span is changed to the largest supported value and IsZoom is set to False.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also