Keysight 89600 VSA .NET API
ResBWNearest Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Frequency Class : ResBWNearest Method


value
Specifies the resolution bandwidth value.

Glossary Item Box

Returns the nearest 1-3-10 step RBW if arbitrary ResBW is disabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function ResBWNearest( _
   ByVal value As Double _
) As Double
C# 
public abstract double ResBWNearest( 
   double value
)
C++/CLI 
public:
abstract double ResBWNearest( 
   double value
) 

Parameters

value
Specifies the resolution bandwidth value.

Return Value

If the IsResBWArbitrary property is set to false, then this function returns the nearest 1-3-10 step. Otherwise, it returns the value.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also