Keysight 89600 VSA .NET API
SetStartStopFrequency Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Frequency Class : SetStartStopFrequency Method


isZoom
Whether the measurement is zoomed or baseband.
startFrequency
Measurement start frequency in Hz.
stopFrequency
Measurement stop frequency in Hz.

Glossary Item Box

Set the measurement IsZoom, Start, and Stop frequency properties all at one time.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SetStartStopFrequency( _
   ByVal isZoom As Boolean, _
   ByVal startFrequency As Double, _
   ByVal stopFrequency As Double _
) 
C# 
public abstract void SetStartStopFrequency( 
   bool isZoom,
   double startFrequency,
   double stopFrequency
)
C++/CLI 
public:
abstract void SetStartStopFrequency( 
   bool isZoom,
   double startFrequency,
   double stopFrequency
) 

Parameters

isZoom
Whether the measurement is zoomed or baseband.
startFrequency
Measurement start frequency in Hz.
stopFrequency
Measurement stop frequency in Hz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also