Keysight 89600 VSA .NET API
SignalTrackChannel Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Frequency Class : SignalTrackChannel Property


Glossary Item Box

Gets or sets which input channel to use for signal tracking.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SignalTrackChannel As Integer
C# 
public abstract int SignalTrackChannel {get; set;}
C++/CLI 
public:
abstract property int SignalTrackChannel {
   int get();
   void set (    int value);
}

Remarks

This setting is ignored unless IsSignalTrack is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also