Keysight 89600 VSA .NET API
ConnectionState Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > HardwareConfiguration Class : ConnectionState Property


Glossary Item Box

Gets the current state of the connection to the hardware within the configuration.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property ConnectionState As ConnectionStateType
C# 
public abstract ConnectionStateType ConnectionState {get;}
C++/CLI 
public:
abstract property ConnectionStateType ConnectionState {
   ConnectionStateType get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also