Keysight 89600 VSA .NET API
ExternalReferenceFrequency Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > HardwareConfiguration Class : ExternalReferenceFrequency Property


Glossary Item Box

Gets or sets the frequency of the external reference signal

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ExternalReferenceFrequency As Double
C# 
public abstract double ExternalReferenceFrequency {get; set;}
C++/CLI 
public:
abstract property double ExternalReferenceFrequency {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also