Keysight 89600 VSA .NET API
IChangeGroup Interface Members
See Also  Methods 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : IChangeGroup Interface

Glossary Item Box

The following tables list the members exposed by IChangeGroup.

Public Methods

 NameDescriptionMinimum SW Version
 MethodDisposePerforms application-defined tasks associated with freeing, releasing, or resetting unmanaged resources. (Inherited from System.IDisposable)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also