Keysight 89600 VSA .NET API
ItemPropertyChanged Event
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ICollectionBase Interface : ItemPropertyChanged Event


Glossary Item Box

Indicates which item in the collection had a property change on it.

Syntax

Visual Basic (Declaration) 
Event ItemPropertyChanged As PropertyChangedEventHandler
C# 
event PropertyChangedEventHandler ItemPropertyChanged
C++/CLI 
event PropertyChangedEventHandler^ ItemPropertyChanged

Event Data

The event handler receives an argument of type PropertyChangedEventArgs containing data related to this event. The following PropertyChangedEventArgs properties provide information specific to this event.

PropertyDescription
PropertyName  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00

See Also