Keysight 89600 VSA .NET API
Enabled Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ICustomStep Interface : Enabled Property


Glossary Item Box

Gets or sets a value indicating whether the step is enabled.

Syntax

Visual Basic (Declaration) 
Property Enabled As Boolean
C# 
bool Enabled {get; set;}
C++/CLI 
property bool Enabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also