Event just before the step is connected to the measurement list (before its InputNames are used).
Syntax
Event Data
The event handler receives an argument of type CustomStepNamingEventArgs containing data related to this event. The following CustomStepNamingEventArgs properties provide information specific to this event.
| Property | Description |
|---|
| DataNames | Gets the list of valid DataNames for this measurement. |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also