Keysight 89600 VSA .NET API
IQNoiseCorrectionMode Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : IQNoiseCorrectionMode Enumeration


Glossary Item Box

Specifies which noise to correct.

Syntax

Visual Basic (Declaration) 
Public Enum IQNoiseCorrectionMode 
   Inherits System.Enum
C# 
public enum IQNoiseCorrectionMode : System.Enum 
C++/CLI 
public enum class IQNoiseCorrectionMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
NoneBasically a pass-through mode; no noise correction is applied.—
UncorrelatedAnalyzerNoiseOnly the uncorrelated (e.g. thermal) Analyzer noise is corrected.—
UncorrelatedDutAndAnalyzerNoiseBoth the DUT and Analyzer uncorrelated (e.g. thermal) noise are corrected.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.40

See Also