Keysight 89600 VSA .NET API
IQNoiseCorrectionSignalMode Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : IQNoiseCorrectionSignalMode Enumeration


Glossary Item Box

Specifies the type of signal being measured.

Syntax

Visual Basic (Declaration) 
Public Enum IQNoiseCorrectionSignalMode 
   Inherits System.Enum
C# 
public enum IQNoiseCorrectionSignalMode : System.Enum 
C++/CLI 
public enum class IQNoiseCorrectionSignalMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BurstedThe signal consists of bursts (with idle periods between bursts).—
ContinuousThe signal is transmitted continuously at a constant repetition rate.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also