This event is used internally to propagate
System.ComponentModel.INotifyPropertyChanged.PropertyChanged events across the remoting boundary. See
NotifyPropertyChangedWrapper for a description of how to receive
System.ComponentModel.INotifyPropertyChanged.PropertyChanged events for a given object.
Syntax
Event Data
The event handler receives an argument of type RemotePropertyChangedEventArgs containing data related to this event. The following RemotePropertyChangedEventArgs properties provide information specific to this event.
| Property | Description |
|---|
| PropertyName | Gets the name of the property value whose name has changed. |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also