Keysight 89600 VSA .NET API
Value(String,Object) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > IStateDictionary Interface > Value Method : Value(String,Object) Method


key
The key name.
defaultValue
The value to return if there is no value in state for the specified key.

Glossary Item Box

Gets an object type value associated with a specified key.

Syntax

Visual Basic (Declaration) 
Overloads Function Value( _
   ByVal key As String, _
   ByVal defaultValue As Object _
) As Object
C# 
object Value( 
   string key,
   object defaultValue
)
C++/CLI 
Object^ Value( 
   String^ key,
   Object^ defaultValue
) 

Parameters

key
The key name.
defaultValue
The value to return if there is no value in state for the specified key.

Return Value

The value in state if it exists; otherwise the defaultValue.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also