Keysight 89600 VSA .NET API
IStepValue Interface Members
See Also  Properties  Methods 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : IStepValue Interface

Glossary Item Box

The following tables list the members exposed by IStepValue.

Public Properties

 NameDescriptionMinimum SW Version
 PropertyMaxValueGets the maximum value.  —
 PropertyMinValueGets the minimum value.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
 MethodStepDownGet the suggested value one step down from the specified value.  —
 MethodStepUpGets the suggested value one step up from the specified value.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also