| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Slope As TriggerSlope | |
| C# | |
|---|---|
public abstract TriggerSlope Slope {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property TriggerSlope Slope { TriggerSlope get(); void set ( TriggerSlope value); } | |
Determine the current trigger slope; either a positive transition from below the trigger level to above it, or a negative transition from above the trigger level to below it. The trigger slope is not used for the free run trigger type.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)