Keysight 89600 VSA .NET API
InputDataDomain Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputDataDomain Enumeration


Glossary Item Box

An enumeration describing the type of input data that a measurement requires.

Syntax

Visual Basic (Declaration) 
Public Enum InputDataDomain 
   Inherits System.Enum
C# 
public enum InputDataDomain : System.Enum 
C++/CLI 
public enum class InputDataDomain : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
SpectrumThe measurement requires magnitude frequency data.—
TimeThe measurement requires time data (the default).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.50

See Also