Keysight 89600 VSA .NET API
InputExtensionChannelCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputExtensionChannelCollection Class


Glossary Item Box

Represents a collection of input extension channel objects.

Object Model

InputExtensionChannelCollection ClassInputExtensionChannel ClassChannelId Structure

Syntax

Remarks

The input extension channel collection contains a collection of input extension channel objects. It contains one input extension channel object per active physical channel within the HardwareGroup in Measurement.SelectedAnalyzer.Groups.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also