Parameters
- name
- The key name of the parameter.
Return Value
The value of the specified parameter.Note: It is recommended to use the strongly typed methods and properties on sub-classes of this class instead of this method. See the specific Input Extension class for the hardware that is being used.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)