Keysight 89600 VSA .NET API
InputExtensionCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputExtensionCollection Class


Glossary Item Box

Represents a collection of input extensions. Represents a collection of input extensions.

Object Model

InputExtensionCollection ClassInputExtension ClassInputExtensionChannelCollection ClassInputExtensionChannel Class

Syntax

Remarks

The input extension collection contains a collection of input extension objects. It contains one input extension object per HardwareGroup in Measurement.SelectedAnalyzer.Groups. An input extension is unique to the specific kind of hardware used in that group and contains settings that are unique to that hardware.The input extension collection contains a collection of input extension objects. It contains one input extension object per HardwareGroup in Measurement.SelectedAnalyzer.Groups. An input extension is unique to the specific kind of hardware used in that group and contains settings that are unique to that hardware.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also