Keysight 89600 VSA .NET API
InputExtensionCoupling Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : InputExtensionCoupling Enumeration


Glossary Item Box

Specifies the behavior of the input extension state when using sequential input channels.

Syntax

Visual Basic (Declaration) 
Public Enum InputExtensionCoupling 
   Inherits System.Enum
C# 
public enum InputExtensionCoupling : System.Enum 
C++/CLI 
public enum class InputExtensionCoupling : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AcrossAcquisitionsSpecifies that parameters be coupled across all acquisitions where the logical instrument index associated with the parameter is the same as the one being changed.—
AllSpecifies that parameters be coupled within an acquisition and across acquisitions (so coupled across all).—
InAcquisitionSpecifies that parameters be coupled within the same acquisition but not across acquisitions.—
UncoupledSpecifies that parameters are uncoupled if possible.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also