Gets the acquisition index that this input extension is a part of when using sequential input channel configurations.
Syntax
| Visual Basic (Declaration) | |
|---|
Public ReadOnly Property AcquisitionIndex As Integer |
| C# | |
|---|
public int AcquisitionIndex {get;} |
| C++/CLI | |
|---|
public:
property int AcquisitionIndex {
int get();
} |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 25.00
See Also