| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Length As Double | |
| C# | |
|---|---|
public abstract double Length {get; set;} | |
This is ignored when gating is disabled. For power spectrum measurements if the specified RBW cannot be realized with the specified gate length then the gate length used by the measurement will be coerced. The ActualLength property will return the actual coerced length and this property will retain the original requested gate length.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.50