Keysight 89600 VSA .NET API
InstrumentType Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > InstrumentId Structure : InstrumentType Property


Glossary Item Box

Gets the instrument type for this instrument. A instrument may be capable of more than one type.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property InstrumentType As InstrumentType
C# 
public InstrumentType InstrumentType {get;}
C++/CLI 
public:
property InstrumentType InstrumentType {
   InstrumentType get();
}

Remarks

The Adc type is used for instruments from which time domain data is read. That usually means an instrument that digitizes (A/D) the signal, but it could be from simulation software (such as for the User input functionality) or from a logic analyzer. An instrument may contain tuner (down converter) or input (calibrator) functionality in addition to an A/D converter. But, if that instrument will be performing the A/D operation then the type should be specified as Adc.

An instrument may be capable of more than one type. For example a Spectrum Analyzer may be used as an Adc type or as a Tuner type depending upon whether that functionality is supported or not with that hardware. When used as a tuner then it is just used as a down converter and some other instrument is used to digitize the signal.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also