Keysight 89600 VSA .NET API
LicenseFeatureException Class Members
See Also  Properties  Methods 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : LicenseFeatureException Class

Glossary Item Box

The following tables list the members exposed by LicenseFeatureException.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorLicenseFeatureException ConstructorOverloaded.   —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDataGets a collection of key/value pairs that provide additional user-defined information about the exception. (Inherited from System.Exception)—
Public PropertyFeatureGets the feature.  —
Public PropertyHelpLinkGets or sets a link to the help file associated with this exception. (Inherited from System.Exception)—
Public PropertyHResultGets or sets HRESULT, a coded numerical value that is assigned to a specific exception. (Inherited from System.Exception)—
Public PropertyInnerExceptionGets the System.Exception instance that caused the current exception. (Inherited from System.Exception)—
Public PropertyMessageGets a message that describes the current exception. (Inherited from System.Exception)—
Public PropertySourceGets or sets the name of the application or the object that causes the error. (Inherited from System.Exception)—
Public PropertyStackTraceGets a string representation of the immediate frames on the call stack. (Inherited from System.Exception)—
Public PropertyTargetSiteGets the method that throws the current exception. (Inherited from System.Exception)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodGetBaseExceptionWhen overridden in a derived class, returns the System.Exception that is the root cause of one or more subsequent exceptions. (Inherited from System.Exception)—
Public MethodGetObjectDataOverridden. Populates a SerializationInfo object with the data needed to serialize the object.  —
Public MethodGetTypeGets the runtime type of the current instance. (Inherited from System.Exception)—
Public MethodToStringCreates and returns a string representation of the current exception. (Inherited from System.Exception)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also