Keysight 89600 VSA .NET API
Contains Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > LimitLineCollection Class : Contains Method


item
The LimitLine to find.

Glossary Item Box

Returns true if the passes LimitLine is in the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Contains( _
   ByVal item As LimitLine _
) As Boolean
C# 
public abstract bool Contains( 
   LimitLine item
)
C++/CLI 
public:
abstract bool Contains( 
   LimitLine^ item
) 

Parameters

item
The LimitLine to find.

Return Value

Return true if the LimitLine is in the collection

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also