Keysight 89600 VSA .NET API
Create Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > LimitLineCollection Class : Create Method


Glossary Item Box

Creates a new LimitLine.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Create() As LimitLine
C# 
public abstract LimitLine Create()
C++/CLI 
public:
abstract LimitLine^ Create(); 

Return Value

A handle to the new LimitLine.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also