| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property SelectedItem As LimitLine | |
| C# | |
|---|---|
public abstract LimitLine SelectedItem {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property LimitLine^ SelectedItem { LimitLine^ get(); void set ( LimitLine^ value); } | |
The selected limit line is the one being edited. Returns null if no limit line is selected.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)