Keysight 89600 VSA .NET API
LimitLineDraw Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : LimitLineDraw Enumeration


Glossary Item Box

Specifies whether the limit is one continuous line or a set of connected dots.

Syntax

Visual Basic (Declaration) 
Public Enum LimitLineDraw 
   Inherits System.Enum
C# 
public enum LimitLineDraw : System.Enum 
C++/CLI 
public enum class LimitLineDraw : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
ConnectedPointsSpecifies set of connected dots.—
OneLineSpecifies one continuous line.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also