Keysight 89600 VSA .NET API
LimitLineTraceFail Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : LimitLineTraceFail Enumeration


Glossary Item Box

Specifies the trace color for failed limit line regions.

Syntax

Visual Basic (Declaration) 
Public Enum LimitLineTraceFail 
   Inherits System.Enum
C# 
public enum LimitLineTraceFail : System.Enum 
C++/CLI 
public enum class LimitLineTraceFail : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
InFailColor>Draw the failure region in the limit line fail color.—
InTraceColorDraw the failure region in the trace color.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also