| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub AddPoints( _ ByVal x() As Double, _ ByVal y() As Double, _ ByVal isConnect() As Boolean _ ) | |
| C++/CLI | |
|---|---|
public: abstract void AddPoints( array<double>^ x, array<double>^ y, array<bool>^ isConnect ) | |
Parameters
- x
- X points.
- y
- Y points.
- isConnect
- Connect points.
The points are inserted into the limit line in ascending X-value order. Any new points are inserted after any existing points with the same X values. The x, y, and isConnect arrays must all be the same size.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)