Keysight 89600 VSA .NET API
YMargin Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > LimitLine Class : YMargin Property


Glossary Item Box

Gets or sets the Y offset between the limit line and the margin line.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property YMargin As Double
C# 
public abstract double YMargin {get; set;}
C++/CLI 
public:
abstract property double YMargin {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also