Keysight 89600 VSA .NET API
Item(String) Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > LimitTestCollection Class > Item Property : Item(String) Property


name
The name of the limit test to retrieve. The name is case sensitive.

Glossary Item Box

Returns the named limit test from the collection.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride ReadOnly Property Item( _
   ByVal name As String _
) As LimitTest
C# 
public abstract LimitTest Item( 
   string name
) {get;}
C++/CLI 
public:
abstract property LimitTest^ Item {
   LimitTest^ get(String^ name);
}

Parameters

name
The name of the limit test to retrieve. The name is case sensitive.

Property Value

The named limit test, or null if no limit test of the supplied name exists.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also