| Visual Basic (Declaration) | |
|---|---|
Public Structure LogicalChannelId Inherits System.ValueType | |
| C# | |
|---|---|
public struct LogicalChannelId : System.ValueType | |
| C++/CLI | |
|---|---|
public value class LogicalChannelId : public System.ValueType | |
The Input.ChangeLogicalChannels method takes an argument(s) of this structure in order to specify specific channels to use. Each logical channel object in the Input.LogicalChannels collection has an Id property that uses this structure.
The structure uniquely identifies a specific logical channel for the current hardware configuration. This identification is unique within the context of the kind of hardware configuration being used. The value of this structure may usually be used with different models of instruments as long as those instruments are from the same family or series. However, a LogicalChannelId from one kind of instrument may mean something totally different in another kind of instrument.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)