Keysight 89600 VSA .NET API
SupportsDotNet Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MacroCollection Class : SupportsDotNet Property


Glossary Item Box

Gets or sets a value indicating whether new or recorded macros should support .NET 6.0 or greater.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SupportsDotNet As Boolean
C# 
public virtual bool SupportsDotNet {get; set;}
C++/CLI 
public:
virtual property bool SupportsDotNet {
   bool get();
   void set (    bool value);
}

Remarks

The .NET SDK to use is available using the DotNetVersion property.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also