Keysight 89600 VSA .NET API
SupportsDotNetFramework Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MacroCollection Class : SupportsDotNetFramework Property


Glossary Item Box

Gets or sets a value indicating whether new or recorded macros should support .NET Framework.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SupportsDotNetFramework As Boolean
C# 
public virtual bool SupportsDotNetFramework {get; set;}
C++/CLI 
public:
virtual property bool SupportsDotNetFramework {
   bool get();
   void set (    bool value);
}

Remarks

.NET 4.8 is the only version of .NET Framework that is supported.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00

See Also