Keysight 89600 VSA .NET API
IsRunning Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Macro Class : IsRunning Property


Glossary Item Box

Gets a value indicating whether the macro is currently running or not.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property IsRunning As Boolean
C# 
public abstract bool IsRunning {get;}
C++/CLI 
public:
abstract property bool IsRunning {
   bool get();
}

Remarks

Macros run on a background thread.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also