| Visual Basic (Declaration) | |
|---|---|
Public Overridable ReadOnly Property TerminationStatus As Exception | |
| C# | |
|---|---|
public virtual Exception TerminationStatus {get;} | |
| C++/CLI | |
|---|---|
public: virtual property Exception^ TerminationStatus { Exception^ get(); } | |
If the previous run terminated without error, null is returned. Otherwise, the exception that caused the macro to terminate is returned.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 14.00